- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Check In Dialog Box
Use this dialog box to check in a file.
Parameters
Parameter | Description |
---|---|
Comments | Enter a comment up to 255 characters in length. Comments longer than 255 characters are truncated. |
Local copy | Select arrow to choose an option:
|
COK | Start the check in process. |
Cancel | Close the dialog box without completing the check in operation. |
Help | Displays help on the Check In dialog box. |
Provide Feedback