Open an existing project

Use this procedure to open a project.
To open an existing project
  1. From the
    File
    menu, choose
    Open
    .
    In the
    Open/Import Project
    dialog box, the project directory configured in the
    Workstation Options
    dialog box opens. If the project file is in another directory, browse to the correct directory.
    In
    File name
    , enter the name of the project file to open or select the file in the browser.
  2. Select
    Open
    to open the project file.
    Once the project file opens, the
    Controller Organizer
    opens. The
    Controller Organizer
    shows everything in the controller at the time the project file was last saved.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.