Save a Project File With a New Name
To save the project file to a different file using a new name:
TIP:
This does NOT change the name of the controller. To change the controller name, change the name on the General tab of the Controller Properties dialog.
- FromSave, select the directory to save this project.
- InFile name, enter the new name.
- FromSave as type, select the file type.Choose from:
- Logix Designer Project File (*.ACD, *.L5K, .L5X, *XML)
- Logix Designer Import/Export File (*.L5K. .L5X, *XML)
- SelectSaveto export the specified file or to save the file with the new name.TIP:To create a backup copy of your project file, save to the hard drive. Copy the saved file to the DVD, using Windows Explorer or another file management tool.For best results, only work on the project files from the hard drive.
Accessing the Save As dialog
- From theFilemenu, selectSave As.
Provide Feedback