Open Instruction Logic command

Open Instruction Logic command

Choose this command to view the logic that the Add-On Instruction is using.
TIP:
Cannot edit logic online, when logic is in the context of an instruction call, or if the instruction is source-protected or sealed with an instruction signature.
A source-protected Add-On Instruction is either locked or read-only. Any part of an Add-On Instruction that is locked cannot be edited, and a locked instruction’s associated logic, local tags, or scan mode routine configuration is not viewable. In addition, any part of an Add-On Instruction that is read-only is not editable. However, all associated logic, local tags, and configuration of a read-only instruction are viewable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.