Failed to save changes

Failed to save changes

There is a problem in trying to save changes to the Add-On Instruction.
The number of InOut parameters exceeds maximum 64
The maximum number of InOut parameters has been reached for the Add-On Instruction. The
Logix Designer
application limits the number of InOut parameters for Add-On Instructions to 64. Remove InOut parameters until number does not exceed the 64 maximum allowed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal