Instruction-based alarms

Use instruction-based alarms to insert alarms in routines or Add-On Instructions.
Logix Designer
supports these types of instruction-based alarms:
  • Analog alarms. An analog alarm defines a condition that evaluates a single analog tag against up to four limit values (high-high, hi, low, and low-low) and up to two rate of change limits (positive and negative). Use the ALMA instruction to implement this type of alarm.
  • Digital alarms. A digital alarm monitors a tag for alarm conditions based on whether the tag is equal or not equal to zero. Each value represent a specific alarm condition. Use the ALMD instruction to implement this type of alarm.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.