Select the units for feedback configuration

Select the units for feedback configuration

Use the tables as a guide when selecting the units for a feedback configuration:
Motor Type
Feedback Configuration
Feedback 1 Units
Rotary PM/Induction
Motor/Load/Dual
Rev
Linear PM/Induction
Motor
Meter
No Motor (Feedback Only)
Master Feedback
Rev/Meter
None
Motor/Load/Dual
Rev/Meter
Motor Type
Feedback Configuration
Feedback 2 Units
Rotary PM/Induction
Load/Dual
Rev/Meter
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal