Position Loop page

Use the settings on the
Position Loop
page in the
Axis Properties
dialog box to configure the position loop of the axis.
TIP:
To open the Position Loop page:
  1. In the
    Controller Organizer
    , expand the
    Motion Groups
    folder, then right-click the axis and select
    Properties
    .
  2. From the
    Axis Properties
    dialog box, in
    Categories
    , select
    Position Loop
    .
Parameter
Description
Bandwidth
Enter a bandwidth value in Hertz.
Integrator Bandwidth
Enter an integrator bandwidth value in Hertz.
Integrator Hold
Enable or disable for the integrator during commanded motion.
Velocity Feedforward
Enter a percentage for the Velocity Feedforward.
Error Tolerance Limit
Enter a value for the position error tolerance in Position Units.
Lock Tolerance
Enter a value for the position lock tolerance in Position Units.
Parameters
Opens the
Motion Axis Parameters
page to modify existing or additional parameters.
Tip:
The
Parameter List
page may contain more attributes than the associated page. In some cases, attributes that display on the
Parameter List
page do not display on the associated page.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.