Workstation Options dialog box overview

Workstation Options dialog box overview

The Workstation Options dialog lets you customize the behavior and appearance of the Logix Designer application.
TIP:
If
FactoryTalk Security
is enabled, this dialog box may appear dimmed, depending on the levels of access that have been defined. For details about
FactoryTalk Security
see
FactoryTalk
Help:
Start > Programs >
Rockwell Software
>
FactoryTalk
Tools >
FactoryTalk
Help
.
This dialog has these parameters:
Parameters
Description
Categories
A list of all options categories that can be configured. Select a category and its options appear to the right of the list. When you change an option, a "*" is appended to the name of the category. You can change options from as many categories as you wish. Press Apply or OK to save your changes.
Reset Category
Click this button to return to the factory default settings for the selected category. Not all categories support this behavior; if you select a category that does not, the button appears dimmed.
OK
Click this button to accept your changes and close the Workstation Options dialog box.
Cancel
Click this button to cancel your changes and close the Workstation Options dialog box.
Apply
Click this button to apply your changes and continue editing in the Workstation Options dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.