Failed to modify trend properties - number of captures out of range

The
Number of Captures
is invalid. The valid range is from a low of 1 capture to a high of 100 captures. Enter a valid
Number of Captures.
TIP:
This control is not active until a
Stop Trigger
value is specified.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.