Controller Properties dialog box - General tab settings

Controller Properties dialog box - General tab settings

The
General
settings on the
Controller Properties
dialog box define the name, vendor, description, revisions of the controller, and other physical properties of the controller.
Settings that do not apply to the controller are hidden.
The ability to change the settings on this tab can be controlled by
FactoryTalk Security
permissions.
Parameter
Description
Vendor
The name of the controller's manufacturer.
Type
The catalog number and description of the controller. When online, the catalog number of the memory card (if any) is included.
Revision
The major and minor revisions of the controller.
If the project has never been downloaded to the controller, this field displays the minimum minor revision required in order to download. Once a project is downloaded to the controller, this field displays the minor revision of the controller.
Name
The name of the controller. The name must be IEC_1131 compliant. If an invalid character is entered in this field, or if the name exceeds 40 characters, the software ignores the character. The name cannot be changed when online.
When the project is created, this is the name of the project file. If the name is changed, the name of the project file does not change. To keep the two the same, then rename the project file using Windows Explorer or select
Save As
from the
File
menu in the
Logix Designer
application.
Description
A description for the controller, up to 128 characters. If the description exceeds the maximum length, the software ignores any extra characters.
The description can be downloaded to the controller and can be added, changed, and deleted when online.
Chassis Type
The chassis type in which the controller resides. The chassis type cannot be changed when online.
This parameter is not available for
CompactLogix
and Compact
GuardLogix
controllers since these controllers do not have a physical chassis.
Expansion I/O
The number of local input and output modules for the controller. When counting the number of input and output modules, do not include the 1769-L1x controller or the single embedded Point I/O module in the count.
This parameter is available only for 1769-L1x
CompactLogix
controllers.
IMPORTANT:
The Expansion I/O must match the number of physical Expansion I/O modules or the controller cannot connect to any local I/O.
Slot
The chassis slot number in which the controller resides. The slot number can only be changed when the controller is offline.
In
ControlLogix
, controllers occupy a numbered slot in the chassis and can be placed in any slot. It is also possible to place multiple controllers in the same chassis.
For
CompactLogix
and Compact
GuardLogix
Safety controllers, because the controller always resides in slot 0, this field is unavailable, and slot number 0 is displayed.
For
GuardLogix
5570 Safety controllers, valid values range from 0 to two less than the number of slots in the chassis (for example, in a 10-slot chassis, valid values range from 0 to 8.)
For
GuardLogix
5580 Safety controllers, the range depends on the safety level:
  • SIL2/PLd safety level - valid values range from 0 to one less than the number of slots in the chassis
  • SIL3/PLe safety level - valid values range from 0 to two less than the number of slots in the chassis
Safety Partner Slot
The location of the Safety Partner for the
GuardLogix
5570 Safety controller and the
GuardLogix
5580 Safety controller when the safety level is SIL3/PLe.
These controllers require two slots: 1 for the Primary controller, and 1 for the Safety Partner. These slots must be side by side, with the partner always in the slot to the right of the primary controller. This parameter is read-only and the value is always equal to the value you entered in the
Slot
plus 1. For example, if you entered a value of 1 in
Slot
, the
Safety Partner Slot
value is equal to 2.
TIP:
Depending on the controller and the safety level, the
Safety Partner Slot
displays <N/A> if there is no safety partner or  <Internal> if the safety partner is internal.
Change Controller
Opens the
Change Controller Type
dialog box to change the controller to another controller, or change the revision within the same platform (for example, changing from a 1769-L33ER controller to a 1769-L36ERM controller) or to another platform.
Attention:
A safety controller cannot change to a standard controller if the project contains safety Add-On Instructions. Either convert the safety Add-On Instructions to standard Add-On Instructions or delete the safety Add-On Instructions from the project.
EtherNet/IP Mode
Shows the EtherNet/IP Mode for the Ethernet ports on the controller. This parameter is available only for controllers that support one or more configurable Ethernet port pairs, for example, the
CompactLogix
5380 and
CompactLogix
5480 controllers.
  • A1/A2: Dual-IP
    - Both ports of the configurable pair reside on separate Ethernet networks, each with its own IP address. All Ethernet ports on the controller share a single domain name and DNS server address configuration. For
    CompactLogix
    5380 controllers, port A1 provides this information and for
    CompactLogix
    5480 controllers, port B1 provides this information.
    L5K_dual_ IP_ mode
  • A1/A2: Linear/DLR
    - Both ports of the configurable pair reside on the same Ethernet network as a single logical node.
    L5K_Linear_DLR_mode
Change IP Mode
Opens the
Change EtherNet/IP Mode
dialog box to change the
EtherNet/IP Mode
setting. This setting is available only for controllers that support one or more configurable Ethernet port pairs, and when the controller is offline.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal