Add a No phase step
Add a No phase step to:
- Prevent sequence steps (in simultaneous divergences and convergences) from starting or stopping at the same time.
- Maintain a consistentEquipment Sequencepattern of step-transition-step.
- Separate adjacent branching structures.
To add a No phase step:
- Select in the Sequence Editor workspace, or select on an element to connect to in the sequence diagram.
- On theEquipment SequenceElement toolbar, selectAdd Disconnected Step
.
- (optional) Right-click the existing link and then clickDeleteto remove any existing links from the element connectors.
- Click the connector of the first element to create a link, and then click the connector of the second element to attach the link.
- Double-click the phase name to display the phase selector, then select<No phase>from the list.
Provide Feedback