SequenceManager Controls

SequenceManager Controls

The
SequenceManager
ActiveX controls provide operator visualization of the
Equipment Sequence
program. There are three operator controls for viewing and interacting with the
Equipment Sequence
s.
The
Sequence Detail Control
provides the operator with a detailed view of an Equipment Sequence, including its chart structure, steps, and transitions. The runtime status of the sequence program and its sequence elements are also shown. The operator can command the Equipment Sequence from this control.
The
Sequence Summary Control
displays the sequence program status for each of the Equipment Sequences downloaded to the controller. The Sequence Summary Control also allow the operator to view and command a selected Equipment Sequence.
The
Sequence Parameters Control
displays a table of all sequence parameters and step tags of a specified Equipment Sequence, and allows the operator to command a selected sequence parameter or step tag. To refine the display, configure the table to filter the information displayed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal