New Equipment Sequence dialog box
Use the
New
dialog box to define the name, description, containing task, and revision information of a new Equipment Sequence. Equipment Sequences can be created only while offline.Equipment Sequence
TIP:
To open the dialog box, on the menu bar, click .
New Equipment Sequence
File > New Component > Equipment Sequence
After you create a new Equipment Sequence, a new
Diagram
routine is added to the Equipment Sequence Editor and an initial step, a transition, and a final step is added to the editor workspace for your diagram. You can add and connect additional sequence elements and branch structures to the existing preliminary diagram to construct a complete Equipment Sequence diagram. Provide Feedback