Copy Equipment Sequence elements
Copy
Equipment Sequence
elements to another location in the current diagram, or to another Equipment Sequence
diagram.To copy
Equipment Sequence
elements:- Select one or more elements.
- On the Menu bar, selectEdit > Copy Element.
- Move the copied element(s) to the desired location.TIP:Also copyEquipment Sequenceelements using these methods:
- Right click on a step and chooseCopy Element.
- With a step selected, use keyboard shortcutCtrl + C.
- With a step selected, useCopyon the main toolbar.
Provide Feedback