What is pasted when sequence elements are cut or copied?
When pasting a step that was cut or copied, and the pasted step name is the same as an existing step in the sequence, a new name is auto-generated by the system.
- If the existing name is a system-generated default, such as Step_000, the new name increments the integer value, becoming in this case Step_001.
- If the existing name is a custom name, an (incremented) integer is appended to the custom name. For example, MyStep becomes MyStep1.
Provide Feedback