Construct an Equipment Sequence diagram with a simple series topology
This example shows how to create, construct, and configure an
Equipment Sequence
diagram that uses a series topology. Before you begin
- Go offline with the controller.
- Create anyEquipment Phases needed for theEquipment Sequence.
- Define a newEquipment Sequence.
- Configure theEquipment Sequenceproperties.
To construct an
Equipment Sequence
diagram with a simple series topology: - Select theSequence Editorworkspace.
- On theEquipment SequenceElement toolbar, selectAdd Step and Transition Pair
.
- Select the connector of the first element to create a link, and then select the connector of the second element to attach the link.TIP:Select the initial step link before adding the step and transition pair and the link automatically connects to the pair.
- Continue toAdd Step and Transition Pairelements as needed.
- Assign a name and a phase to each step.
- Create transition expressions between each step.
- Continue adding steps and transitions as needed.
- Connect to the end step
.
- Verify the routine:
- In the Standard toolbar, select
.
- Errors are listed in the Output window on theErrorstab at the bottom of the application.
Provide Feedback