Equipment Sequence Properties - Monitor tab fields

Use the
Monitor
tab of the
Equipment Sequence Properties
dialog to view run-time information of the Equipment Sequence, including maximum and last scan times, the current sequence state, and its owner. These options are available on the
Monitor
tab.
L5K_SILC_Equipment Sequence_MonitorTab
Item
Name
Purpose
1
Max
Displays the maximum amount of scan time of the Equipment Sequence, in microseconds.
Important:
When the
Equipment Sequence
scan rate is significantly longer than the
Equipment Phase
scan rate, sequence events triggered by step state changes may not be generated. If having those event records is necessary, it is advisable to avoid phase state changes occurring in less than the sequence scan rate.
2
Last
Displays the last scan time of the Equipment Sequence, in microseconds.
3
Reset Max
This button resets the maximum and last scan times and restarts the scan timer.
4
State
Shows the current state of the Equipment Sequence. Available states are: IDLE, COMPLETE, STOPPED, ABORTED, HELD, RESETTING, STOPPING, RUNNING, ABORTING, HOLDING, and RESTARTING.
5
Substate
Shows the current substate for pausing of the Equipment Sequence. Available substates are:
  • <No Display>
  • Pause Enabled
  • Paused
  • Auto Pause Enabled
  • Paused, Auto Pause Enabled
6
Mode
Shows the current mode for the
Equipment Sequence
. Available modes are:
  • Automatic
  • Manual
7
Owners
Shows the current owner(s) of the Equipment Sequence. Owners are users or programs that have the right to command an
Equipment Sequence
or
Equipment Phase
. Owners can be instances of Logix Designer, internal sequencers, operators, and external sequencers.
Available owners are:
  • Internal Sequencer
  • External Sequencer
  • Operator
  • The
    Logix Designer
    application (#) - where # is a count of separate
    Logix Designer
    applications overriding ownership
8
Unit ID
The Unit ID is a numerical representation of the piece of equipment an
Equipment Sequence
is controlling. For example, a factory might have two identical mixers, MIXER_A (ID = 26) and MIXER_B (ID = 35). The sequence executes, and the generated events are archived. Reports created from that sequence event data identify which mixer was used (UNIT ID = 35).
9
Sequence ID
A user-generated identifier assigned to each execution of an
Equipment Sequence
so the
Equipment Sequence
and the events it generates can be recognized for display, analysis, and reporting purposes.
OK
Select to accept edits. If all attributes are valid, the modified attributes are saved for the current Equipment Sequence and this dialog box closes.
OK
and
Apply
are unavailable if the dialog box contains invalid data.
Cancel
Select to cancel edits and close the
Equipment Sequence Properties
dialog box.
Apply
Select to apply edits and continue editing in the
Equipment Sequence Properties
dialog box. Applying edits runs the same validation as clicking
OK
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.