Monitor Equipment Sequence run-time information
Monitor an dialog box.
Equipment Sequence
in the Monitor
tab of the Equipment Sequence
PropertiesBefore you begin:
- Make sure the controller is offline.
- Access theEquipment Sequenceby right-clicking on anEquipment Sequenceand selectingProperties, or by double-clicking anEquipment Sequencein theController Organizer.
To monitor an
Equipment Sequence
:- Select theMonitortab.
- View theScan times
- Max: Displays the maximum amount of scan time of theEquipment Sequence, in milliseconds.
- Last: Displays the last scan time of theEquipment Sequence, in milliseconds.To reset theMaxandLastscan times, and restart the scan timer, selectReset Max.
- View theStateandSubstate
- State: Displays the current state of theEquipment Sequence: IDLE, COMPLETE, STOPPED, ABORTED, HELD, RESETTING, STOPPING, RUNNING, ABORTING, HOLDING, and RESTARTING.
- Substate: Displays the current pause substate of theEquipment Sequence: <No Display>; Pausing; Paused; Pausing, Auto Pause; and Paused, Auto Pause.
- View theOwners. Owners are users or programs that have the right to command anEquipment Sequence. Owners can be instances ofLogix Designer, Sequence Graphic Elements, and other programs.
- If reseting the scan times, selectApply, thenOK. Otherwise selectCancel.
Provide Feedback