Change sheet layout size and orientation

Change sheet layout size and orientation

Specify the sheet size and orientation for the selected
Equipment Sequence
in the
Routine Properties
dialog box
Sheet Layout
tab. Change all sheets within an
Equipment Sequence
from this tab.
To specify the sheet size and orientation for a selected routine:
  1. Go offline with the controller.
  2. From the
    Sheet size
    menu, choose the size of the sheet to use for this routine.
  3. Select the sheet orientation to use for this routine:
    Landscape
    (the default setting) or
    Portrait
    .
  4. Select
    OK
    to apply the edits and close the
    Routine Properties
    dialog box.
    TIP:
    The sheet size of a routine contains a margin around the sheet. This margin is equal to 1/2-inch, or the minimum value supported by your printer, whichever is greater, plus the header and footer region. Therefore, the actual sheet size available for a routine is the size chosen from the
    Sheet
    size menu, minus the size of the margin. This is the actual area in which logic is rendered.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.