Failed to set the Bit Number

Failed to set the Bit Number

You tried to set the value of the tag in the
Configuration
dialog box, but the operation did not succeed. This value represents a bit of a tag structure member. You might see this error when you select
Apply
, press Enter, or move off of one of the fields with a blue arrow. This could occur because:
  • The tag was deleted.
  • There is an invalid numeric value for the type of field (that is, if the field is expecting an integer and you enter a real value).
  • Insufficient memory.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.