PowerFlex

PowerFlex

Data exchange support for PowerFlex devices:
PowerFlex 
Catalog Number or Product Family
RDF support
AML support
22C...
No
No
22N...
No
No
25*
Yes
Yes
PowerFlex 523 drives
Partial
1 2
Partial
1 2
PowerFlex 525 drives
Partial
1 3
Partial
1 3
PowerFlex 527-STO CIP Safety drive
Partial
1
Partial
1
PowerFlex 700
No
No
PowerFlex 753 drives
Partial
1 4
Partial
1 4
PowerFlex 755 drives
Partial
1 5
Partial
1 5
DriveLogix 57*
No
No
PowerFlex 4 Class Multi*
No
No
PowerFlex 400*
No
No
PowerFlex 40*
No
No
PowerFlex 4*
No
No
PowerFlex 523-C
No
No
PowerFlex 523-E*
Yes
Yes
PowerFlex 525-C
No
No
PowerFlex 525-E*
Yes
Yes
PowerFlex 527-STO CIP Safety
Yes
Yes
PowerFlex 70 ED*
No
No
PowerFlex 700 AC*
No
No
PowerFlex 700 Vector*
No
No
PowerFlex 7000*
No
No
PowerFlex 700*
No
No
PowerFlex 70*
No
No
PowerFlex 753-CNETC
No
No
PowerFlex 753-ENETR
Yes
Yes
PowerFlex 753-NET-C
No
No
PowerFlex 753-NET-E
Yes
Yes
PowerFlex 753-NET-Q
No
No
PowerFlex 755 HiPwr-PMM-EENET
No
No
PowerFlex 755 HiPwr-CNETC
No
No
PowerFlex 755 HiPwr-EENET
Yes
Yes
PowerFlex 755 HiPwr-ENETR
Yes
Yes
PowerFlex 755 HiPwr-NET-C
No
No
PowerFlex 755 HiPwr-NET-E
Yes
Yes
PowerFlex 755 HiPwr-NET-Q
No
No
PowerFlex 755 PMM-EENET
No
No
PowerFlex 755-CNETC
No
No
PowerFlex 755-EENET*
Yes
Yes
PowerFlex 755-ENETR
Yes
Yes
PowerFlex 755 HiPwr-EENET-CM*
Yes
Yes
PowerFlex 755-NET-C
No
No
PowerFlex 755-NET-E
Yes
Yes
PowerFlex 755-NET-Q
No
No
PowerFlex 755T*
No
No
PowerFlex 755 DC FC*
No
No
PowerFlex 755 DC*
No
No
*
All devices of type
1
Configuration properties not fully supported.
2
PowerFlex 523-E2P drive imports as a type PowerFlex 523-E drive but includes the PowerFlex 523-E2P description in the configuration properties.
3
PowerFlex 525-E drive imports as a type PowerFlex 523-E drive and includes the PowerFlex 523-E description in the configuration properties.
PowerFlex 525-E2P drive imports as a type PowerFlex 525-EENET drive but includes the PowerFlex 525-E2P description in the configuration properties.
PowerFlex 525-EENET-Multi drive imports as a type PowerFlex 525-EENET drive but includes the PowerFlex 525-EENET-Multi description in the configuration properties.
4
PowerFlex 753-NET-E drive imports as a type PowerFlex 753-ENETR drive but includes the PowerFlex 753-NET-E description in the configuration properties.
5
PowerFlex 755 HiPwr-ENETR2 drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755 HiPwr-ENETR description in the configuration properties.
PowerFlex 755 HiPwr-NET-E drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755 HiPwr-NET-E description in the configuration properties.
PowerFlex 755-EENET drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-EENET description in the configuration properties.
PowerFlex 755-ENETR drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-ENETR description in the configuration properties.
PowerFlex 755-EENET-CM drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-EENET-CM description in the configuration properties.
PowerFlex 755-EENET-CM -S drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-EENET-CM-S description in the configuration properties.
PowerFlex 755-EENET-CM-S1 drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-EENET-CM-S1 description in the configuration properties.
PowerFlex 755-HiPwr-EENET-CM drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-HiPwr-EENET-CM description in the configuration properties.
PowerFlex 755-HiPwr-EENET-CM-S drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-HiPwr-EENET-CM-S description in the configuration properties.
PowerFlex 755-HiPwr-EENET-CM-S1 drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-HiPwr-EENET-CM-S1 description in the configuration properties.
PowerFlex 755-NET-E drive imports as a type PowerFlex 755 HiPwr-EENET drive but includes the PowerFlex 755-NET-E description in the configuration properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal