Select a project controller

Select a project controller

Rockwell Automation systems hardware diagrams as represented in CAD tools may have multiple controllers. Use the
Select Project Controller
dialog box to select a project controller for the import of data into a new
Logix Designer
application.
Before you begin:
  • Select a data exchange file (.aml or .rdf) to import into the project. For a description of these file types, see
    Data exchange with other software applications
    .
To select a project controller:
  1. In the
    Select Project Controller
    dialog box, examine the list of controllers and their properties.
  2. Select a controller. The selected controller becomes the project controller in the
    Logix Designer
    application. The project controller contains the tags, tasks, programs, and all other components that control devices within the I/O configuration.
  3. Select
    Next
    to go to the
    Select Modules
    dialog box
    to choose modules, and the modules' CIP topology, to include in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal