Failed to modify password
A problem occurred when attempting to change the password. The error message indicates one of these conditions:
Password type not selected
Did not choose a password to set from the What Password menu. Choose a password and continue.
Invalid password for Old Password
The password entered in the Old Password field is invalid. Enter the password again, being careful to enter proper syntax.
Password mismatch. Old Password does not match current password.
The password entered does not match the currently configured password.
Invalid password for New Password
The password entered in the New Password field is invalid. Enter the password again, being careful to enter proper syntax.
Password mismatch. New Password does not match Confirm New Password.
The password entered as the new password does not match what was entered in the Confirm New Password field. Enter both passwords again, making certain they are the same.
Provide Feedback