Select multiple items in the organizers

You can select multiple items in the
Controller Organizer
or the
Logical Organizer
and then perform open, copy, cut, delete, move, partial export, or other operations on them. You can select multiple items only if they are:
  • Siblings (children of the same parent item), and
  • The same type (for example, programs or User-Defined Data Types).
Items that support multiple selection include:
  • Programs (programs in the
    Controller Organizer
    ; programs and folders in the
    Logical Organizer
    )
  • Add-On Instructions
  • User Defined Data Types, including Strings
Routines, Motion Axes, Trends, and Modules do not allow multiple selection.
To select multiple items in the
Controller Organizer
or the
Logical Organizer
:
To select contiguous items:
  1. Select the first item for the range of items.
  2. SHIFT
    +click the last item of the group. All of the items in the group are highlighted.
To select a non-contiguous group of items:
  1. Select the first item to select it.
  2. CTRL
    +click the next item to add it to the selection. Continue until you have selected all the items.
To deselect an item, press
CTRL
+click.
For more information about the organizers, see:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.