Monitor PINTLK parameter values
Use the
General
tab to monitor the status of Process Interlocks (PINTLK) instructions.To monitor parameter values for Process Interlocks (PINTLK) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- When online with the controller, selectResetto reset all interlocks. The action is immediate if the command request does not need to be confirmed by the operator. If the command request requires a signature, this will enforce security from the HMI and disable the command from the Logix Designer dialog. The button is always disabled when the device is offline.
- Monitor these parameters:
- Interlock bypass status. At the top left, the overall status displaysNot bypassedorBypassed.
- First out. Lists the first Not OK condition.
- Type. The type of each interlock. Configure types on theHMI > Typetab.
- Interlock name. Interlocks configured for the instruction.
- State. The state of each interlock. Possible states are blank,Bypassed, orNot OK.TIP: TheGeneraltab lists interlocks after they are configured on theAdvanced 0-15andAdvanced 16-31tabs.
Provide Feedback