PAIM limits, quality, selection settings
Use the
Advanced
tab on the Properties
dialog box for Process Multi Sensor Analog Input (PAIM) instructions to configure settings for monitoring the input and signal for the sensor process variable (PV).To configure limits, quality, and selection settings for PAIM instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAdvancedtab.
- Configure these settings:SettingDescriptionPV fail highEnter the high limit for input. Input above this limit is reported as poor quality.DeadbandEnter the deadband for the high and low fail limits.Enter the deadband for the high and low fail limits.Use the deadband to select an error range above and below the limits when a failure is not reported. The deadband prevents unwanted rapid switching of the status.PV fail lowEnter the low limit for input. Input below this limit is reported as poor quality.Has inputSelect the check box for each active input signal.Tag nameEnter a label for each signal. The labels appear on the HMI and on theGeneraltab.Use inputSelect the checkbox for each signal to use to calculate the final PV (average or median).PV MaxEnter the maximum value for display of the PV. Values above this maximum are not displayed.PV MinEnter the minimum value for display of the PV. Values below this minimum are not displayed.Minimum number of good inputs for a good PVEnter the number of good inputs required for the PV to pass quality requirements. Inputs must fall within thePV fail highandPV fail lowlimits to be considered good.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device status: PV good, PV uncertain, or PV bad.
- Device issues. Displays fault conditions: None, Any reject, Min good, Fail, or Configuration error.
- SelectApply.
Provide Feedback