HMI navigation for PVLV
Use the
Navigation
tab on the PVLV Properties
dialog box to configure navigation from the HMI to additional objects or destinations for Process Valve (PVLV) instructions.To enable HMI navigation for PVLV instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theHMItab, selectNavigation.
- To allow navigation to an object or destination from the HMI faceplate, selectAllow navigationfor each device.Use theHMI > Command configurationtab to define labels for positions 1 and 2.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current valve state, such asPulse continuouslyorOut of service.
- Device issues. Displays fault conditions, such asFeedback faultorTransit stall.
- SelectApply.
Provide Feedback