Remove Custom Properties for a plug-in
If you uninstall a plug-in or do not want to use it, you can remove all custom properties for that plug-in. When a plug-in is not registered with
Logix Designer
application, removing the custom properties for the plug-in removes the plug-in from the plug-ins list.To remove custom properties for a plug-in:
- On theToolsmenu, clickPlug-In Manager.
- ClickRemove All Custom Properties for Plug-In.
Provide Feedback