- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
SBR/RET Properties dialog box overview
Use
SBR/RET Properties
to set the parameters for the SBR/RET instruction. This element passes and returns parameters to and from a sequential function chart routine when calling it through a JSR instruction.
TIP:
A downloadable SFC routine can have 0 or 1 SBR/RET elements. You can have more in your routines, but you can not download them if multiple elements exist.
Field | Description |
---|---|
Input Parameter | Lists all tag references that receive a value from a corresponding JSR input parameter. You can enter new tag references to the list and modify existing tags. |
Return Parameter | Lists all tag references that send a value to a corresponding JSR return parameter. You can enter new tag references to the list and modify existing tags. |
Provide Feedback