Configure a main routine

Configure a main routine

To execute the logic in a routine when a program is triggered, you must configure the routine to be the main routine for the program. Use the
Configuration
tab of the
Program Properties
dialog box to assign a main routine.
To configure a main routine:
  1. From either the Controller Organizer or Logical Organizer, right-click the program to change and choose
    Properties
    .
  2. Choose the routine to designate as the main routine from the
    Main
    menu in the
    Assigned Routines
    frame.
  3. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.