Background
Since 1983, Automatismes Girona (AUGI) has developed and implemented complete solutions in the field of industrial automation in order to upgrade any kind of machinery and process. Thanks to its diversification, it covers a wide variety of industries such as food and feed, chemical and pharmaceuticals, plastics, healthcare, water treatment and renewable energy.
The company has two relevant certifications, which verifies its professional qualifications. First, the quality management standard ISO 9001, which credits the good practice on all projects. Second, the company is a Rockwell Automation Solution Partner, which means it demonstrates the highest level of commitment to Rockwell Automation technologies and relationships; is an industry leader; and has differentiated services or solutions that complement or extend those of Rockwell Automation.
This recognition is precisely why dozens of customers around the world trust AUGI; with one example being PROAN (PROTEINA ANIMAL, S.A. de C.V.), a Mexican feed manufacturer dedicated to the production of eggs, pork and dairy milk, which decided to automate its entire factory with the help of AUGI and Rockwell Automation.