Source Control > Check In command

Choose this control to initiate the check in operation.
Note that this menu item displays only if all of the following conditions exist:
  • an open project exists
  • either the
    Logix Designer
    application has automatically drawn an association between the open project and one under source control, or you have explicitly established that association;
  • the open project is checked out, the check out belongs to the current user, and the path to the open project matches the checked out path recorded by the source control server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.