System Protocol no broadcasting
The selected protocol in the Controller Properties Dialog Box - System Protocol Tab Overview does not support broadcast messages. To send a broadcast message, the system protocol should be set to DF1 Master, DF1 Radio Modem, or DF1 Slave.
NOTE:
Logix Designer versions 37 and later do not support controllers with serial ports. The
System Protocol
tab appears only in Logix Designer versions 36 and earlier for controllers with a serial port.To configure the system protocol for broadcasting
- In theController Organizer, right-click the controller and chooseProperties.
- Select theSystem Protocoltab.
- From theProtocolmenu, chooseDF1 Master,DF1 Radio Modem, orDF1 Slave.
Provide Feedback