Configure programs
Use the
Program Properties
Configuration
dialog box to assign routines and, under specific conditions, inhibit a program and synchronize redundancy data after execution.To configure programs:
- From theProgram propertiesdialog box, select theConfigurationtab.
- Select theMainroutine assigned to the program.
- Select theFaultroutine assigned to the program.
- SelectInhibit Programto prevent the controller from executing this program. The option is cleared by default.This option is disabled if theUse as Foldercheck box is selected on theGeneraltab.
- SelectSynchronize Redundancy Data after Executionto synchronize data at the end of the program execution.This option is disabled when:
- theUse as Foldercheck box is selected on theGeneraltab
- when Redundancy is not enabled
This option does not appear for Safety controllers. The option is always enabled for controllers with Redundancy enabled as long as the controller is not in Hard Run mode. - SelectOKto save the program properties.
Provide Feedback