Display multiple active alarms for an object
At runtime, if the same alarm activates repeatedly, the
Alarm grid
widget displays the most recent alarm event. Use branching to display multiple active alarms for the same alarm object.In the
Alarm grid
widget, all active alarms for the same alarm object appear and must be acknowledged and confirmed. Alarm events do not occur when variables return to normal status in the controller. Rockwell Automation
recommends branching when a project requires rigorous control and alarm count. For example, use branching in production processes for products that are subject to certification, such as medical products.- At the top ofProject view, select the main project node
.
- InProperties, expandAlarm configuration, and then inBranching enabled, selectTrue.
Provide Feedback