Alarm events

Each alarm type has a specific event in the
Properties
pane.
There are three default methods for each alarm event:
  • Acknowledge
    . Acknowledge the alarm.
  • Add comment
    . Add a comment to the alarm in the alarm grid.
  • Confirm
    . Resolve the cause of the alarm.
TIP: Supported AlarmCondition event methods for a selected item in the alarm grid include only Acknowledge, Confirm, and AddComment in the current release. The Dynamic Links browser displays additional methods when expanding AlarmGrid > Selected Item > AlarmCondition which will be supported in a future release.
Alarm type
Alarm event
Digital alarm
OffNormalAlarmType
Exclusive level alarm
ExclusiveLevelAlarmType
Exclusive deviation alarm
ExclusiveDeviationAlarmType
Exclusive rate of change alarm
ExclusiveRateOfChangeAlarmType
Non-exclusive level alarm
NonExclusiveLevelAlarmType
Non-exclusive deviation alarm
NonExclusiveDeviationAlarmType
Non-exclusive rate of change alarm
NonExclusiveRateOfChangeAlarmType
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.