Alarm variables

Each alarm type has variables that you can dynamically link to the property of a graphic element. When the configured level for a graphic object is reached and the alarm occurs, the graphic object displays the value or message of the configured alarm.
For example, you can create a digital alarm and link the
Active
property of a graphic object such as a light-emitting diode (LED) to the
Active
variable of the digital alarm. When the alarm becomes active, the LED turns on.  
Available variables depend on alarm type.
Alarm variables
Alarm variable
Description
Included in alarm types
Active
Make the graphic object active
All alarm types
Auto acknowledge
Acknowledge the alarm without intervention from the user
All alarm types
Auto confirm
Confirm the alarm without intervention from the user
All alarm types
Enabled
Enable the alarm
All alarm types
High limit
Indicate that the high limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
High-high limit
Indicate that the high-high limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Input variable
Input the value from the Input value of the graphic element
All alarm types
Low limit
Indicate that the low limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Low-low limit
Indicate that the low-low limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Max TimedShelve duration
Indicate the maximum duration of TimedShelve
All alarm types
Message
Display the configured message when the alarm is active
All alarm types
Message high-high state
Display the configured message when the alarm is active and the high-high limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Message high state
Display the configured message when the alarm is active and the high limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Message low-low state
Display the configured message when the alarm is active and the low-low limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Message low state
Display the configured message when the alarm is active and the low limit of the graphic object is reached
Exclusive and Non-Exclusive alarm types
Normal state value
Specify the normal value for the monitored variable. The alarm activates when the value of this variable is different from the one specified.
Digital alarm only
Polling time
Specify how frequently to poll for the status of the alarm
Exclusive Rate Or Change and Non-Exclusive Rate of Change alarms
Preset TimedShelve duration
Indicate the default TimedShelve duration for the alarm
Severity
Display the severity of the alarm
All alarm types
Setpoint value
The desired value for the monitored variable.
Exclusive Level Deviation and Non-Exclusive Level Deviations alarms
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.