Engineering unit converter
Use the engineering unit converter to convert raw data values into scaled values based on a range of customizable values.
TIP:
For example, the engineering unit converter can transform values from 0 to 65.535 supplied by a temperature sensor into corresponding values on a scale from -20 to +70. The input of an engineering unit converter is generally a dynamic link to an imported tag.
Properties
Property | Description |
---|---|
Raw min | Minimum raw data value. |
Raw max | Maximum raw data value. |
Scaled min | Minimum converted value. |
Scaled max | Maximum converted value. |
Mode | The direction of the dynamic link:
|
IMPORTANT:
The converter does not operate if you do not specify values in the
Raw min
and Raw max
properties and there is no dynamic link for the input variable.If... | Then... |
---|---|
Raw min and Raw max properties are not set. | The converter assumes that there is an analog variable set in the input via a dynamic link. Raw min and Raw max are set to Low limit and High limit of the input analog variable respectively. |
Raw min and Raw max properties are set. | The converter considers Raw min and Raw max properties and ignores any Low limit and High limit values of the analog variable input. |
Only Raw min or Raw max property is set. | The converter assumes that there is an analog variable set in the input via a dynamic link and ignores the Raw min and Raw max properties. Raw min and Raw max are set to Low limit and High limit of the input analog variable respectively. |
Source
A variable that contains a raw value to be converted.
Output
A scaled value based on the configured linear conversion.
Example
![](/content/dam/dita/en/factorytalk-optix/current/_images/converter_engineering_unit.png/_jcr_content/renditions/original)
Provide Feedback