Direct Drives Connectivity

Use Direct Drive Connectivity feature in your projects to enable PowerFlex drives.
The Direct Drive Connectivity allows to:
  • Create information model of PowerFlex, basing on drive predefined profiles
  • Create client and read data from PowerFlex drives. Four types of PowerFlex drives are supported: PF755, PF755TM, PF6000T, and PF7000
TIP:
The Direct Drive Connectivity is supported only on Windows®  operating systems.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.