LED
Displays a Boolean value in the form of an on LED or an off LED.
Use case
Signal an alarm status, a mechanical component function, or a software function.
Example
Inactive LED
![Animated graphic showing a red LED light being either on or off](/content/dam/dita/en/factorytalk-optix/current/_images/ref_led_ex.png/_jcr_content/renditions/original)
Active LED
![Animated graphic showing a red LED light being either on or off](/content/dam/dita/en/factorytalk-optix/current/_images/ref_led_ex2.png/_jcr_content/renditions/original)
Provide Feedback