Copy paths to nodes

Copy a path to a single node or copy paths to multiple nodes.
  • To copy a path to a single node:
    1. In
      Project view
      , right-click a node.
    2. Select
      Copy path to node
      .
  • To copy paths to multiple nodes:
    1. In
      Project view
      , while holding the
      keyboard key, select multiple nodes.
    2. Right-click any selected node and select
      Copy paths to nodes
Path to node or paths to nodes are copied to the system clipboard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.