Can't change the properties for axis Axis Tag Name

Can't change the properties for axis
Axis Tag Name
. Please enter an
Attribute Name
between
Minimum Value
and
Maximum Value
.
The value entered is out of range. The minimum and maximum values allowed for the attribute may also depend on other attributes entered. For example, the Home Position attribute should be within the overtravel limits if the limits are used for the axis.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.