GroupFault
GroupFault is a 32-bit attribute. Its value is set upon the occurrence of one of the following faults. Click a fault in the following list for more information about that fault.
To clear a GroupFault:
- Diagnose and fix the underlying problem.
- Be sure your program or fault handling routine contains a Shutdown Reset (MGSR) instruction to return to the axis ready operating state.
Provide Feedback