Source Control > Undo Check Out command
Choose this command to initiate the undo check out operation.
Note that this menu item displays only if all of the following conditions exist:
- an open project exists
- either the Logix Designer application has automatically drawn an association between the open project and one under source control, or you have explicitly established that association;
- the open project is checked out, the check out belongs to the current user, and the path to the open project matches the checked out path recorded by the source control server.
Provide Feedback