Overview
This course introduces the student to single and three-phase A.C circuits and shows how to draw and perform calculations for each type of circuit.
This course introduces the student to single and three-phase A.C circuits and shows how to draw and perform calculations for each type of circuit.
There are no prerequisites for this course.
Electrical Technician
Calculate electrical values of single-phase A.C. circuits.
Draw single-phase A.C. circuits.
Calculate electrical values of three-phase electrical circuits.
Draw three-phase A.C. circuits.
Identify and build single-phase A.C. circuits.
Identify and explain the common connections used to build three-phase A.C. circuits.