The KVC Smart Pump Control, built on the technology of Rockwell Automation, made its debut in Malaysia at the largest water and wastewater event for developing Asia - the Asia Water Expo 2018, held in April at the Kuala Lumpur Convention Centre.
The pump provides operational excellence with an intelligent motor control system to optimise water delivery. This enables state water operators to maintain sustained water supply to their customers in Malaysia while cutting the cost of power consumption at the same time, thanks to cutting edge technology from Rockwell Automation.
Water operators today face numerous challenges resulting from environmental factors, increasing demand, water wastage or scarcity, as well as costs due to increased energy/electricity prices and overwhelming expenses of repair works and replacements. These factors may be a hindrance to operators who need to ensure maximum efficiency of water distribution, as they can affect the quality and the quantity of water distributed.
However, technology advancements have made possible the development of smart solutions that water operators can leverage to counter some, if not all, of these concerns. The smart pump system through its array of unique and smart features counters these pain points of water distribution companies.