- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
Duplicate a project
Duplicate a project to use an existing project as a template for a new project.
- Open the project to be copied and then from the main menu, selectSave as.
- InSave project as, complete:
- Name. The name of the new project.
- Location. The storage location of the project files. The duplicated project is stored in the same location as the original project by default. Select the folder icon to browse to a new location.
- (optional)Use Source Control. Select to save your project in a Git repository.
- SelectOK.
Provide Feedback