IUANode.Remove(child)

IUANode.Remove(child)

Removes a project node that corresponds to the C# object passed in the argument.
void Remove(IUANode
child
);

Arguments

child
(IUANode)
A C# object that corresponds to the project node to add.

Example

The following example shows that the
MyLabel
label child of the
Panel1
object is removed from the project:
var myPanel = Project.Current.FindObject("Panel1"); var objToRemove = Project.Current.FindObject("MyLabel"); myPanel.Remove(objToRemove);
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.