Create a motor values widget (type)
Create container elements for gauges, labels, and text boxes related with selected motor values.
- Create the motor values widget panel:
- InProject view, right-clickUIand select .
- Hover-over the panel, select, and enterMotorValuesWidget.
- Create an alias to the motor instances:
- InProperties, at the top, selectand selectAlias.
- Double-clickAlias1and enterMotor.
- Create a dynamic link betweenKindandFor more information about dynamic links, see Create dynamic links.
- Create a motor speed panel:
- InProject view, right-clickMotorValuesPanelWidgetand select .
- Hover-over the panel, select, and enterMotorSpeedPanel.
- Create a motor acceleration panel:
- InProject view, right-clickMotorValuesWidgetand select .
- Hover-over the panel, select, and enterMotorAccelerationPanel.
Provide Feedback